5/10/2012 12:57 PM | |
Posts: 2348 Rating: (263)
|
And can you upload project here? Also - what language you used for writing blocks? If it was SCL you can just open files as txt in /s7asrcom folder. |
5/10/2012 1:24 PM | |
Joined: 3/21/2006 Last visit: 4/4/2024 Posts: 10228 Rating: (1181) |
Hello, 1. Can you create and open after a new project? 2. Version of WInCC is... 3. Copy that project ot local hard disk and try it to open from there. 4. In case of need to reinstall the Simatic Manager in order to jump format: procedure -How do you uninstall STEP 7 completely, including all the software packages? Best regards, Hristo Mihalev
|
5/10/2012 5:12 PM | |
Posts: 621 Rating: (10) |
Hi umencho 1 yes i created new project 2 Version of Wincc flexible is sp2 3 yes i cpyed the same project of local hard disk and i was tryed to open 4 procedure also already linked mr darious these are all above i tryed but now facing the second snap which was i attached in this topic |
Follow us on