7/5/2012 2:42 PM | |
Joined: 3/14/2008 Last visit: 5/7/2024 Posts: 2066 Rating: (928) |
Cannot see it in Wincc anymore. The manual: Process Control System PCS7 (Operator station 8.0) is referring to a document: Process Control System PCS 7; Programming Guide for Blocks |
Last edited by: Oreca at: 7/5/2012 2:43 PMIf I could help you, you can use the RATE button. Thank you. |
|
7/9/2012 7:53 AM | |
Joined: 3/14/2008 Last visit: 5/7/2024 Posts: 2066 Rating: (928) |
Ahhh ok got it... I think during my install of 7.1, it was installed automatically... but I found it.. Also, it looks like there are less blocks in the 8.0 library then in the 7.1 version. I cannot see 7.1 library. Do I also need to install it from somewhere? |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on