11/1/2012 9:51 AM | |
Joined: 1/3/2006 Last visit: 2/19/2024 Posts: 726 Rating: (71) |
Hi BitRidder, There is now confusion amd I'am not sure about things. Please see the attached file. There in they have mentioned that all CP1613 software products can be operated with the CP1623. Please help clarify on this.
AttachmentCP1623_Query.pdf (405 Downloads) |
11/1/2012 12:15 PM | |
Joined: 1/3/2006 Last visit: 2/19/2024 Posts: 726 Rating: (71) |
More details: Hardware : CP1623 OS: Windows 2003 R2 SP2, Standard edition PCS7: V6.1 SP3 which comes with Simatic Net V6.3 HF1 From Compatiblity I have found this: ->CP 1623 is compatible with above mentioned OS. ->PCS7 and Simatic Net is not compatible with above OS, instead they are compatible withWindows 2003 Standard Edition SP1. Now what we can conclude from thisabout CP1623 compatiblity? (Supporting file attached) Attachmentcompatiblity_CP1623.pdf (319 Downloads) |
11/1/2012 4:39 PM | |
Joined: 6/18/2008 Last visit: 8/13/2020 Posts: 14 Rating: (1) |
Hi Manmeet, You cannot use a CP1623 with PCS7 v6.1! See this link: https://support.automation.siemens.com/WW/adsearch/resultset.aspx?region=WW&lang=en&netmode=intranet&ui=NDAwMDAxOAAA&term=Restricted+Delivery+Release+for+the+SIMATIC+NET+PC+CP1623+Module&ID=28402000&ehbid=28402000 It says: "The only precondition is the use of the SIMATIC NET CD with version 2007 + Hotfix 1 or higher." |
Kind regards, |
|
This contribution was helpful to1 thankful Users |
11/1/2012 5:42 PM | |
Joined: 1/3/2006 Last visit: 2/19/2024 Posts: 726 Rating: (71) |
Ok BitRidder, So we need Simatic Net 2007+HF1 on a machine with CP1623. So here is the another googly question: What if I install Simatic Net 2007 on Windows server 2003 R2 Standard Edition?They are compatible! Also does Simatic Net contains the driver for running CP1623? Anyways thanks for getting it clarified. Regards, Manmeet.
|
Follow us on