1/9/2013 9:08 AM | |
Joined: 10/10/2005 Last visit: 4/18/2024 Posts: 1917 Rating: (132) |
Hello, you have to install STEP 7 V5.5 first and second the WinCC flexible. Consider the correct software version of WinCC flexible in refer to Windows. See also the informations of the FAQ: http://support.automation.siemens.com/WW/view/de/18734363 With best regards |
1/9/2013 10:01 AM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2683 Rating: (135) |
Thread closed, because question is already discussed in the following thread WinCC Flexible and Step7 Integrated project Best regards O_Moderator |
Follow us on