Industry Online Support
Technical Forum
4/8/2014 12:50 PM | |
Joined: 2/1/2012 Last visit: 3/26/2024 Posts: 9 Rating: (0) |
I have problems to run my stepper motor. I'm using 6ES7138-4DC01-0AB0, and the application is simple, just move forward and backward. In HMI I created two memories, one forward and one backward, and I also have a ruler 0-100%, which is the position feedbak of the stepper motor. I believe that I should set up only for speed, configured this way, but the motor did not move. If possible, I would like an example of how to do this. I'm using Haydon DCM8028 drive. Best Regards.
AttachmentDCM8028DCM8055Manual.pdf (237 Downloads) |
Follow us on