Industry Online Support
Technical Forum
5/26/2014 6:54 AM | |
Joined: 6/8/2013 Last visit: 3/12/2024 Posts: 158 Rating: (9) |
hi, What is the diff. between BACNET ms/tp and ip protocol ? ie. speed , distance Thanks
A. G. Naphade |
5/26/2014 9:50 AM | |
Posts: 12 Rating: (9) |
BACnet ms/tp is a datalink link layer protocol based on EIA-485, cable length depends on used speed, up to 76800 bits per seoconds it is 1200m. For wiring, termination resistors and grounding see attachment. BACnet/P stands for BACnet over Ethernet 802.3., Typical speed is 100 mega bits per seconds. cable length depends ob cable type, typically 100 m AttachmentD:\Downloads\BACnet_Doku\Auszug_Standard_MS_TP.pdf (755 Downloads) |
This contribution was helpful to1 thankful Users |
5/30/2014 6:08 PM | |
Posts: 59 Rating: (1) |
Thank You For PDF Attachment Its USefull FOr US REgard Shailesh |
Follow us on