4/29/2011 8:32 AM | |
Joined: 11/17/2010 Last visit: 11/25/2020 Posts: 81 Rating: (2) |
Hello, Question about WinCC flexible 2008. For my project i want to display the user name in the template screen for the userthat is logged in. So when i use Sm@rt service i can see directly who is logged in on the HMI that is standing by the machine. There are 3 kind of user: Operator, user, and programmer. Is this possible? Also i want to add an logout button in the template screen, that is only visible whenthere is a user logged in. (there are some functionsthat have acces without logging in) Is this possible? Thanks in advance! Nick |
This contribution was helpful to1 thankful Users |
4/29/2011 9:24 AM | |
Joined: 4/29/2010 Last visit: 8/12/2024 Posts: 1557 Rating: (161)
|
Hello, this is really easy. Go to the scheduler at your project and add a new job. Take a look at the attached screenshots and do it like that. best regards Attachmentscheduler.zip (2749 Downloads) |
This contribution was helpful to10 thankful Users |
9/11/2014 10:26 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
Follow up question published by vperezbis split to a separate thread with the subject Display user name. Best regards Min_Moderator |
Follow us on