12/9/2014 8:22 PM | |
Posts: 12 Rating: (0) |
I am trying to connect Siemens S7300 (CPU 314 IFM) with Siemens TP170A Touch panel via MPI communication. I need to show value from a sensor on the touch panel via output tag. I get the value from the sensor in the Step 7 but i cannot get that value on the touch panel. I don't know what am i doing wrong beacuse i always get zero value. I maked the printscreens from configuration. Can someone please look at the pictures and tell me what am i doing wrong. (I am using ProTool Lite which is integrated in Simatic Manager)
AttachmentTP170A.zip (277 Downloads) |
12/10/2014 3:30 PM | |
Posts: 12 Rating: (0) |
thank you for the reply, i tryed to change Address to ''2'' in Peer Parameters but nothing happened, i again get 0 value on the panel, when i changed Expansion Slot to ''2'' also i get some weird numbers on the panel (see the pictures). What could be the problem?
AttachmentTP170A 2nd try.zip (203 Downloads) |
12/10/2014 4:06 PM | |
Posts: 12 Rating: (0) |
thank you, now is working |
Follow us on