Industry Online Support
Technical Forum
1/3/2011 10:52 AM | |
Posts: 45 Rating: (4) |
Hello hanjorre, It seems that you are using Win7 64-bit, you must use 32-bit instead. please check this post: https://www.automation.siemens.com/tf/WW/en/Posts/50779 Hope this will help |
2/1/2011 3:50 PM | |
Posts: 510 Rating: (117) |
I have attached the Operating System document. Ultimate N is not specified but it is not excluded. On the Microsft website I found an update to upgrade the N and KN versions to standad Ultimate. http://www.microsoft.com/downloads/details.aspx?displaylang=en&FamilyID=31017ed3-166a-4c75-b90c-a6cef9b414c4 Also, in the OS document it specifies that the Flexible 2008 SP2 is compatible with IE V6.0 SP1, V7.0 and V8.0. If Internet Explorer is not installed on your system you may need to add it as well. Good Luck, billwest
Attachment22055368_WinCC_flexible_MS_BS_2008_V1_1_e.pdf (1040 Downloads) |
6/29/2014 9:45 PM | |
Posts: 5 Rating: (0) |
Try this one /tf/WW/en/Posts/35429
|
Follow us on