1/22/2015 8:53 AM | |
Joined: 3/14/2008 Last visit: 4/18/2024 Posts: 2064 Rating: (926) |
Hello dzwilu, I also tried setup a SFC type and reproduce the problem...can't do it. 1. You can try to make a screenshot for us when all your I/O isvisible in CFC. Maybeyou somehow disabled manual control. 2. If it is some sort of bug, I suggest to insert a new instance and justdrag the interconnections to the "faulty" instance to the new one.. also adjust your parameter values.Then do a compile+download change and check again if it is working then. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on