6/8/2012 12:27 PM | |
Posts: 3037 Rating: (192)
|
Hello, You find mre information about WinCC flexible and S7 1200 in the following FAQ. How do you access S7-1200 tags with a panel or RT configured with WinCC flexible 2008 SP2? Tweety |
This contribution was helpful to1 thankful Users |
6/12/2012 3:28 PM | |
Posts: 3037 Rating: (192)
|
Hello Kolma, How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI? Have you an access point for each connection in the PC/PG interface? See the screenshot Tweety |
1/21/2014 12:40 PM | |
Posts: 340 Rating: (6) |
follow up question published by Ammieis split to a seperate thread with the subject Communication between S7-1200 and WinCC flexible 2008 SP3 - SP2 works |
Follow us on