4/27/2015 4:49 AM | |
Joined: 1/30/2013 Last visit: 10/1/2022 Posts: 13 Rating: (1) |
I also get the same problem with my Function Blocks. I am working on TIA V13 SP1 update 1 PLCs I use are S7-300, and S7-1200 and the bug applies to both PLCs. When the inputs and outputs of a block are too many, it will not return an ENO=1. I have another block with only 4 outputs, and it returned ENO=1.
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 4/28/2015 10:44:40 AMNew subject after splitting |
|
Follow us on