7/15/2013 6:14 AM | |
Joined: 5/12/2006 Last visit: 4/23/2024 Posts: 22224 Rating: (2979)
|
Hello, which Version do you install exactly? On which point of the installation you get the freeze? Regards Christoph |
7/15/2013 8:42 AM | |
Joined: 3/21/2006 Last visit: 4/4/2024 Posts: 10228 Rating: (1181) |
Do you have another Siemens software installed there? |
This contribution was helpful to1 thankful Users |
8/9/2013 5:02 PM | |
Joined: 1/30/2009 Last visit: 4/22/2024 Posts: 18 Rating: (1) |
Hi Please see attached. I will also put screen shot of errors when i try to launch Scout. Language is set to default - English. THANKS. AttachmentInstallScoutLog.zip (188 Downloads) |
8/9/2013 5:08 PM | |
Joined: 1/30/2009 Last visit: 4/22/2024 Posts: 18 Rating: (1) |
hI Please see attached. When i try to launch Scout, i get these 3 errors. After acknowledging it, the scout opens up. But then i can not open an existing project or create a new project. Attachmentscout errors on VM first 3 errors when launching.zip (159 Downloads) |
5/5/2015 4:29 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4775 Rating: (123) |
|
Follow us on