6/3/2015 4:45 PM | |
Joined: 4/25/2012 Last visit: 6/25/2024 Posts: 28 Rating: (7) |
Dear Denilson How is the memory utilization of S7-1500 family when compared with S7-300/400. For instance, a project using 300 k bytes of work memory in a S7-300 will use about the same amount of memory in a S7-1500 cpu. Best Regards Célio Ricardo Quaio Goetten Softenge Automação Industrial
--------- |
Last edited by: CS Moderator at: 6/6/2015 8:18:28 AMsplitting |
|
6/5/2015 1:08 PM | |
Joined: 9/23/2005 Last visit: 9/25/2024 Posts: 4347 Rating: (1446) |
Hi, E.g. the instructions should use same number of bytes, however, I don't know a exact rule to compare both type of memories. You should take in account that S7-1200/S7-1500 save the comments and symbolic names and S7-300/S7-400 not (it could makes, by itself, a big difference). Other point is that with only symbolic (optimized access) the DB/FB takes less space in S7-1200/S7-1500 compared with S7-300/S7-400.
An general compare was published in https://support.industry.siemens.com/tf/ww/en/posts/88783/ |
Denilson Pegaia |
|
6/5/2015 8:24 PM | |
Joined: 4/25/2012 Last visit: 6/25/2024 Posts: 28 Rating: (7) |
The file with the comparison between the CPUs is exactly what I was looking for. Thanks Denilson! |
6/7/2015 6:49 PM | |
Joined: 9/23/2005 Last visit: 9/25/2024 Posts: 4347 Rating: (1446)
|
You are wellconme :) |
Denilson Pegaia |
|
Follow us on