6/2/2015 12:05 PM | |
Joined: 8/3/2009 Last visit: 9/20/2024 Posts: 13753 Rating: (1735) |
Hello stevom Which Panel do you use in your WinCC flexible Project? Scripts can only be used in Multi Panels or Panels >=277 or in WinCC flexible Runtime. When you use a Panel or a Runtime which are able to do scripting you can try the following FAQ to Reset WinCC Flexible: https://support.industry.siemens.com/cs/ww/en/view/36645252 If nothing helps please send us a screenshot of your Project Tree. Good Luck Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on