6/22/2015 9:37 AM | |
Joined: 6/3/2009 Last visit: 9/14/2022 Posts: 118 Rating: (2) |
Hello, I have a configuration like this: 1. CPU 416-3FS06-0AB0 (400 Safety) 2. IM 151-8FB01-0AB0 (ET200S Safety) 3. 158-0AD01-0XA0 (DP/DP Coupler) I have made the configuration in both CPUs and every thing seems fine, everything on the DP/DP coupler is green. In both PLCs I have put FB223 and FB224 communication block to exchange data. In the 400 I have everything ok, on the FB223 and FB224 there is no error, on the 300 on the FB224 (F_SNDDP) there is no error but on the FB223 (F_RCVDP) I have error=1 and DIAG: B#16#10 in HEX format. The DP_DP and LADDR adresses are coresponding according to what is send in one CPU is recieve in another CPU and vise versa. In attach I'm sending some pics from blocks online and HW configuration.
Thanks in advance AttachmentScreenshots.zip (211 Downloads) |
Last edited by: Min_Moderator at: 6/22/2015 1:01:08 PMMove pictures to attachment |
|
6/29/2015 11:50 AM | |
Joined: 6/3/2009 Last visit: 9/14/2022 Posts: 118 Rating: (2) |
Hello, anyone to have some suggestions? Thanks |
Follow us on