7/3/2015 3:55 PM | |
Posts: 5225 Rating: (1185) |
maybe add this too.. (use one of the two) |
This contribution was helpful to1 thankful Users |
7/4/2015 7:23 AM | |
Joined: 6/26/2013 Last visit: 4/17/2024 Posts: 17 Rating: (0) |
I have connected 13 bit encoder output to directly to input port of PLC (I0.0, I0.1, I0.2 ... I1.4) and also I have read the digital inputs by saving to Memory (MW1) bit by bit. refer to atachment photos. my problem is: when I rotate encoder's shaft the inputs of PLC doesn't change at all. please refer to enclosed attachment. (project photos) regards Ahmad AttachmentProject_photos.rar (604 Downloads) |
Follow us on