7/2/2015 9:33 AM | |
Joined: 7/4/2014 Last visit: 8/9/2024 Posts: 283 Rating: (0) |
Dear Sir Subject machine was not in use for few months. We had battery alarm, we replaced in power ON condition. Since then we started having "Communication Error" and hence all LEDs on MCP keep blinking As per the standard procedure, we erased NC and PLC both then loaded NC and PLC NC side looks OK as we can see all axes on Machine screen but Error 2001 PLC has not started up We uploaded PLC to find only system data, DB15 Request to confirm of attached file, which actually had extension.arc, renamed as .zip is valid one or not Kindly advice AttachmentPLCSDB13082014.zip (205 Downloads) |
Follow us on