7/3/2015 3:18 PM | |
Joined: 5/7/2015 Last visit: 9/20/2023 Posts: 56 Rating: (1) |
Hi Denilson, I have made a face-plate for an ON-OFF valve that we use -about 60- in my current project. I wish now to make a pop-up screen associated with the above face-plate so that this pop-up uses the same interfaces as the valve face-plate. PS. I have used Schneider's vijeo citect in the past. The equivalent of your faceplate is called a 'genie' and that of a dynamically tagged pop-up is called a super-genie. When a genie is associated witha super-genie it takes on the tags of the genie when invoked.
------------- |
Last edited by: CS Moderator at: 7/3/2015 4:11:21 PMnew subject after splitting |
|
7/6/2015 9:33 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4776 Rating: (123) |
|
Follow us on