7/20/2015 4:57 PM | |
Joined: 6/24/2013 Last visit: 4/25/2024 Posts: 1590 Rating: (409) |
Hi You can do something similar to FC attached to this post. address is input to the FC. telegram structure is in local variables. input data from drive copied to local variables in bulk output copied from local to the drive PQWs in bulk too everything is accessed through named, local variables. the working function was used for Sinamics drive and can be modified to different telegram (set of information exchanged with the drive) remember to make sure telegram in drive is consistent with its image used in Your FC. AttachmentFC19_GU120_drive_telegram_20.pdf (105 Downloads) |
Follow us on