7/21/2015 9:24 PM | |
Posts: 1 Rating: (0) |
Hi, I have a problem with a simovert vc drive as well. I am getting F044 mostly at the first powering up of the drive. The drive is used on a shiploader to lower and raise an arm. Once we reset the My CU2 module is 6SE7090-0XX84-0AF0 + 6SE 7090-0XX84-0AJ0. I tried to replace the cards (CU2) however I am unable to estabish communication with my siemens PG hence I can't download the parameters. I have no problem communicating with the existing CU2 module. I need to establish communication, please can you give me some guidelines. Regards
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 7/23/2015 11:24:52 AMNew subject after splitting |
|
7/24/2015 10:22 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
|
Follow us on