7/27/2015 7:22 AM | |
Posts: 1 Rating: (0) |
Dear sir I have step 7 version 5.5 installed .I have to build a step 7 program hardware with Scalance 6GK5 788 2AA60 6AA0 v 4.2.4 , but it does not exist in the HW catalog of my step 7 . While Scalance 6GK5 788 2AA60 6AA0 v 4.0 and Scalance 6GK5 788 2AA60 6AA0 v 4.3 exist .How can I get Scalance 6GK5 788 2AA60 6AA0 v 4.2.4 in my step 7 HW catalog .So please help me . Regards Shyam
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 7/27/2015 3:33:10 PMNew subject after splitting |
|
7/27/2015 9:55 AM | |
Joined: 5/12/2006 Last visit: 4/24/2024 Posts: 22226 Rating: (2980) |
Hello, SCALANCE W700 and STEP 7The Ethernet interface can be configured in STEP 7 if the following requirements are met:
The diagnostics functions can also be used. The WLAN interface cannot be configured with STEP 7. so please update to Step7 V5.5 SP4 and download the GSDML from the WebInterface of the Scalance switch and install it in Step7 HWCOnfig.
Christoph |
Last edited by: ChristophD at: 7/27/2015 9:56:04 AMLast edited by: ChristophD at: 7/27/2015 9:57:09 AM |
|
Follow us on