8/18/2015 4:26 PM | |
Posts: 5 Rating: (0) |
hi How i can replace the motherboard of the PC Panel ?? i replace it but the windows dose not start?? the system of the panel is Win NT4 |
8/24/2015 11:02 PM | |
Posts: 5 Rating: (0) |
Hello ...sorry for my late i replace the board with PC Panel 870 board |
8/25/2015 4:40 AM | |
Joined: 5/12/2006 Last visit: 9/18/2024 Posts: 22364 Rating: (3011) |
Hello, and the original was also a IPC 870? Christoph |
8/26/2015 11:13 AM | |
Posts: 5 Rating: (0) |
Hello no the original was pc panel 670 and yes I can see the BIOS screen |
8/26/2015 1:03 PM | |
Posts: 5 Rating: (0) |
Hello the system on the H.D.D is win NT 4 and After the system boot it show a blue screen and this massage Win NT 4 sp6 and thenthe system freeze best regards |
8/26/2015 1:34 PM | |
Joined: 5/12/2006 Last visit: 9/18/2024 Posts: 22364 Rating: (3011) |
Hello, in this case with NT4 no way without reinstalling the operation system. Regards Christoph |
Follow us on