Industry Online Support
Technical Forum
9/13/2015 3:28 AM | |
Joined: 10/12/2014 Last visit: 9/19/2024 Posts: 66 Rating: (0) |
sir ; i m from sri lanka .I m working as a engineer in our company . Here i attached the error code image which is appeared in the Simatic panel .In simatic panel stop button also blinking . In this situation when I try to download the backup program , I cant proceed ,because when downloading the program using simatic manager it gives another error.Here i also attached the simatic manager error code image which appeared in the program. sir please help me to overcome with this fault. ------------------------------------------------------------------------------------------ Attachmenterror.zip (376 Downloads) |
Last edited by: Min_Moderator at: 9/13/2015 11:52:23 AMNew subject after splitting |
|
Follow us on