Industry Online Support
Technical Forum
10/4/2015 3:41 PM | |
Posts: 9 Rating: (0) |
hello we use g150 j type drive(parallel operation converters),2 winding motor,2 separate line module(AC/DC),two separate MM(DC/AC). while starting the drive unit immediately drive triggering the fault f30002 (Vdc over voltage fault).i done capacitor reforming also.then also i am getting same fault in one motor module only plz find i am attaching drive backup.inform me any parameters want to change Attachment420fn01_29_9_2014.zip (118 Downloads) |
10/6/2015 1:41 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
Closed cause question posted twice. The second thread with the subject G150, Fault f30002 is published within the conference SINAMICS. Best regards Min_Moderator |
Follow us on