5/19/2016 2:15 PM | |
Joined: 12/21/2015 Last visit: 11/22/2023 Posts: 8 Rating: (0) |
Hello, Is the OPC still the only way to communicate with simotion? Regards. |
5/19/2016 2:30 PM | |
Posts: 1529 Rating: (202) |
No. Comfort Panels work fine with SIMOTION. Basic Panels (2nd Gen) will also work if the SIMOTION is the only communication partner. |
5/19/2016 4:51 PM | |
Joined: 12/21/2015 Last visit: 11/22/2023 Posts: 8 Rating: (0) |
What about TIA WinCC RT Professional V13 SP1 |
5/19/2016 7:48 PM | |
Joined: 5/12/2006 Last visit: 4/19/2024 Posts: 22211 Rating: (2979)
|
is the same, it is not working |
Follow us on