2/5/2016 3:55 AM | |
Posts: 153 Rating: (7) |
Dear All I have recieved same problem from 6 customer. 1. When Installing Starter V4.4 SP1 online mode can see the Drive Unit and in offline not possible. installed the same again but same result Solution: unstalled Starter and again installed 4.4 hf3-working fine and can see all. 2.When Installing Starter V4.4 SP1 no possible to install SSP of V4.7 of Sinamics S120 and G120. and SSP for DCM V1.4 Sollution:Solution: unstalled Starter and again installed 4.4 hf3-working fine and can install all SSP. 3.Online help not possible to see. Please note all software installed on windows 7 OS. Please suggest what could be the problem AttachmentStarter Problem.zip (395 Downloads) |
2/13/2016 11:21 PM | |
Joined: 5/21/2015 Last visit: 8/13/2024 Posts: 1 Rating: (0) |
Hi, I installing this SSP SINAMICS S120 Hotfix Package V4.7 and the problem is resolved. |
This contribution was helpful to1 thankful Users |
2/24/2016 3:08 AM | |
Joined: 4/24/2013 Last visit: 3/1/2024 Posts: 8 Rating: (0) |
Thanks for S120, but no S110 in STARTER. I install last HSP for S110. |
Follow us on