2/13/2016 7:47 PM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (307)
|
Hello Please have a look at the following post ( I think that this is what you are looking for ) : Diagnostic package PNIODiag for diagnostic evaluation for PROFIBUS DP and PROFINET IO (STEP 7 V5.x) You can use FB 126 with the standard templates provided to display Profibus diagnostics on HMI I would also recommend you to check out Additional function to filter the FB126 PNIODIAG by IBN_Service. The FC299 provideded by IBN_SERVICE, allows you easier diagnosis of Profibus and Profinet. Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
This contribution was helpful to1 thankful Users |
2/15/2016 10:01 AM | |
Posts: 90 Rating: (0) |
Hello Navnag! I read document and see FB126 do not support for IM151-1. The fault I/O module on DP station could be shown on WinCC? Thanks! |
Follow us on