Industry Online Support
Technical Forum
10/26/2007 9:09 AM | |
Joined: 10/26/2007 Last visit: 11/22/2018 Posts: 4 Rating: (0) |
Hi,I have a project which is upgraded from PCS7 V5.2 to PCS7 V6.1,When we finish the project, we encountered a problem, that is the OS often can not run because the picture is not dynamic and can not select the objects of the picture and the objects of the picture is no response when we click it by the mouse, but the operating system(Windows 2003 Server)is ok. When we restart the computer, the OS is ok again, but It is not ok after sereral days, and we found when the picture is not dynamic and not refreshed by the AS, the Wincc_Sys_02.txt of the Diagnose folderis always writen the following information:255,02.08.2007,00:00:44:484,1007008,4,,SERVER11,SCRIPT,EndAct Timeout. And this problem takes place often when weswitch the pictue. Who can help me analysis the problem, and why,how to do? Thanks a lot! Attachmentdiagnose_server11.zip (455 Downloads) |
Last edited by: yangfl at: 26.10.2007 12:16 |
|
10/30/2007 5:25 AM | |
Joined: 10/26/2007 Last visit: 11/22/2018 Posts: 4 Rating: (0) |
Dear Dec expert: Could pls help analysis what's the problem about the project? Thanks a lot! |
10/30/2007 5:27 AM | |
Joined: 10/26/2007 Last visit: 11/22/2018 Posts: 4 Rating: (0) |
Dear: Any else had seen this problem, and how to do it,why? Thanks a lot!!! |
Follow us on