4/29/2016 12:02 PM | |
Posts: 3093 Rating: (322)
|
Hello Arun, Regards, |
4/29/2016 2:57 PM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (306) |
Hello When you download the Driver to CP341, The driver code is saved in the retentive memory of the CP 341. Generally It is not needed to download this driver again. You can change anytime the communication parameters of the CP which are stored in the Hardware configuration of the CPU. As correctly advised by Craig7 and Kaulquappe you need to look for the problem elsewhere. The Diagnostics buffer is the best starting point. Also check if 24VDC supply to the CP341 module is O.K. besides the points listed by them Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
Follow us on