5/3/2016 2:33 PM | |
Joined: 10/24/2011 Last visit: 3/9/2023 Posts: 257 Rating: (1) |
Hello, I am working on S7-1200 system (CPU 1214C DC/DC/DC). I have used memory card SMC 128C9F2904 (4MB) (6ES7 954-8LC01-0AA0). Now, problem I am facing is that when I try tp download the program with memory card I get error message. I have attached error mesage with thread. (Error number -88). I am unable to reset it also. How to reset memory for S7-1200 CPU?? But when I try downloading without memory card, I can download successfully. What may be the reason?? Also, I want to know, if PLC is power off, for how many days program will be stored in CPU memory (if am not using memory card)??? Thanks, Shailesh AttachmentError in PLC.docx (40 Downloads) |
5/3/2016 2:55 PM | |
Joined: 7/9/2015 Last visit: 5/3/2024 Posts: 3818 Rating: (554) |
Hi, I think you mean this FAQ: How can you delete the IP address and reset your S7-1200 to factory settings using the SIMATIC MC memory card (2MB or 24MB)? Regards |
|
|
5/3/2016 3:01 PM | |
Joined: 7/7/2010 Last visit: 5/3/2024 Posts: 14680 Rating: (2350)
|
II absolutely did not mean that FAQ, but you are looking in the right places.
|
science guy |
|
Follow us on