5/26/2016 1:11 AM | |
Joined: 1/17/2006 Last visit: 8/18/2024 Posts: 553 Rating: (29) |
Hi Oreca. Thanks for the helpful info ! |
"Educate the children and it won't be necessary to punish the men." |
|
5/27/2016 5:51 PM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936)
|
Hi Berg, No, not that I know off. I have to test this...Maybe I can do this tomorrow or this evening. Why? Do you receive errors? and which error exactly? |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
5/27/2016 7:02 PM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936)
|
Ahh OK, I don't think so. When creating custom blocks, the SCL compiler does not check for correct syntax, but when you compile or download the AS program (one of the two, can't remember), an error is displayed that the syntax is wrong. When you did not use: "s7_xm_c", but only "s7_m_c", this means the structure itself is send to the OS, but not the individual parameter like "Value" or "ST". And since you will not use a structure in the faceplate/block icon, but the individual parameter, it will not work. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on