5/28/2016 9:39 AM | |
Posts: 20 Rating: (0) |
Hi, I have bought a 1212c plc, and i can work with it when i connect the plc on the tia portal. Whe i try to work in simulation mode i can not download the software, and it is also not possible to start simulation mode because the start button is gray. i have downloaded the sim s7 1200/1500 simulator on the right way and when i simulate with the 200 or 300 series all works perfect. what do i wrong. grtz frans ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/30/2016 11:30:27 AMNew subject after splitting |
|
Follow us on