7/12/2016 3:41 PM | |
Posts: 75 Rating: (1) |
Hello Friends, I used simple program for run my G120. I succeed run motor via profinet under "G120 -> Commissioning -> Control Panel" manually. But there are 3 func. in main. Parameters, Simulation and Process Data. Which bits and word i must to change in these functions to run the motor. Best Regards.. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 7/12/2016 3:55:18 PMNew subject after splitting |
|
7/19/2016 12:53 PM | |
Posts: 75 Rating: (1) |
Thanks, its work. Where from did you learn this information, is there any document write this ? |
7/19/2016 4:32 PM | |
Posts: 75 Rating: (1) |
Ok, i read again and i understood that. Actually i want to change a parameter's value which i want. For example 1082. How can i do that ? |
7/20/2016 1:43 PM | |
Posts: 75 Rating: (1) |
Thank you for your help.. I am trying to run with sample program (profinet). There are 2 ramp option for change but i want to add a new parameter to control via HMI. For example i want to change drive's max. freq. with use this block. How can i do that, it is the main questoin? AttachmentG120_parameter_add.zip (301 Downloads) |
Follow us on