8/24/2016 11:57 AM | |
Joined: 3/2/2007 Last visit: 4/23/2024 Posts: 928 Rating: (5) |
kindly, we need to use new sinamics motor modules with old control unit cu320. are the below compatible with each other? we are using scout v4.4 new hardware: 1FK7042-2AF71-1BG2 and 1FK7042-2AF71-1CG2 servomotors 6SL3120-2TE13-0AA4 Double Motor Module 6FX5002-2DC10-1CF0 and 6FX8008-1BB11-3AA0 and 6SL3060-4AA50-0AA0 cables old hardware: 6SL3040-0MA00-0AA1 SINAMICS CONTROL UNIT CU320 https://support.industry.siemens.com/cs/pd/484318?pdti=pi&lc=en-QA 6SL3054-0CG01-1AA0 SINAMICS S120 COMPACTFLASH CARD WITH FIRMWARE OPTION PERFORMANCE-EXTENSION 1 INCLUDING CERTIFICATE OF LICENCE V2.6 https://support.industry.siemens.com/cs/pd/246958?pdti=td&lc=en-QA 6AU1445-0AA00-0CA0 SIMOTION DRIVE-BASED MULTIAXES BUNDLE D445 CONSISTING OF 1 UNIT EACH PROGRAMMABLE MOTION CONTROLLER D445 (6AU1445-0AA00-0AA0) + CF (6AU1400-2PA01-0AA0 -Z M44) WITH MULTIAXES PACKAGE LICENSE https://support.industry.siemens.com/cs/pd/23976?pdti=td&lc=en-QA |
Last edited by: Ziemens at: 8/24/2016 12:57:48 PM... thank you ... |
|
8/24/2016 1:34 PM | |
Joined: 3/2/2007 Last visit: 4/23/2024 Posts: 928 Rating: (5) |
do you think we will have any issues with the old Simotion , due to the new motor modules ? thanks |
... thank you ... |
|
8/24/2016 1:39 PM | |
Joined: 5/12/2006 Last visit: 4/25/2024 Posts: 22227 Rating: (2980)
|
Hello, the old simotion use the same logik an FW like the old CU320, so no problem here. Regards Christoph |
10/18/2016 1:42 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
New question published by Badri-UAE is split to a separate thread with the subject CU320 Version E is faulty, can I replace with Version G. Best regards |
Follow us on