8/25/2016 8:45 AM | |
Joined: 1/27/2015 Last visit: 1/24/2024 Posts: 53 Rating: (8) |
Hi Kamil_Sarac, if you want to use Modbus/TCP for communication to Quantum you can use either a CP334-1 or if you have a PN CPU (like 3xx PN/DP) the internal PN Port. For CP you can use Simatic Modbus/TCP CP (2XV9450-1MB00) https://support.industry.siemens.com/cs/ww/en/ps/2XV9450-1MB00 For use with PN CPU you have to use Simatic Modbus/TCP PN-CPU (2XV9450-1MB02) https://support.industry.siemens.com/cs/ww/en/ps/2XV9450-1MB02 There are also sample projects available: https://support.industry.siemens.com/cs/ww/en/view/22660304 Modbus/TCP CP Modbus/TCP PN CPU Regards Bachgeist |
This contribution was helpful to1 thankful Users |
8/25/2016 12:40 PM | |
Joined: 1/27/2015 Last visit: 1/24/2024 Posts: 53 Rating: (8) |
Hi Kamil_Sarac, so you have the Modbus/TCP software already implemented, did the parameterization, you have the T-blocks in your project and all that stuff? Did you know about our sample project? I only can give advice concerning our Siemens Modbus/TCP blocks, because I have no experience with quantum and don't know the system. Sorry, but I try real hard to understand what is your problem and what you want to know. Sample project Modbus/TCP PN: https://support.industry.siemens.com/cs/ww/en/view/22660304 Regards Bachgeist |
Follow us on