8/25/2016 10:23 PM | |
Posts: 5 Rating: (0) |
Hello all, Regarding mySQL or SQL database, i have problems with connection ODBC and TIA runtime Advanced. I'm not sure how to made connection between TIA and SQL, on SQL manager i made database also the same in the ODBC, but i'm not sure where i need to set some setting in TIA. on the forum i found few examples with SQL logging but when i start it i always receive the same error of missing ODBC connection.. Could you please provide me some manual how to setup connection.. for the query.s is not problem, i already made some scripts .. Before Tia Runtime, i was using another scada systems and there was necessary to put database name, port .... but in TIA i didn't find these option .. Also question for the SQL data logging we need some additional licence, because from time to time i receive error that licence key is not available. ps. i'm using Runtime Advanced Probably you have some manual or instructions ... Thanks, Best in advance .. Elvis, ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 8/26/2016 9:35:17 AMNew subject after splitting |
|
8/26/2016 10:57 AM | |
Joined: 6/3/2014 Last visit: 1/17/2023 Posts: 660 Rating: (191) |
Hello eeelvis, do you already know these FAQs?
|
~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
Follow us on