8/29/2016 2:35 PM | |
Joined: 9/1/2015 Last visit: 4/8/2024 Posts: 3 Rating: (0) |
Dear experts, I install WebNavigator V7.4 on one of my servers. Windows Server 2012 R2. I followed the instructions given in manual WinCC V7.4-WinCC Basic Options Section 1.1 and i configure as per instructions the Server and published the pictures successfully. Then i wanted to try if everything is working fine and i download and install WinCCViewer RT on a laptop connected to the same network as the Server. I have connected successfully to the Server but i get a message "The Server is currently in Demo Mode!" and if i press OK on this message the containers are empty. See attached screenshot. I also tried to connect via Internet Explorer but i have the same issue. Containers were empty. I thought that something went wrong at the publishing of the pictures and i published them again with Web View Publisher but i have the same result. Can you please advise a solution to this issue? Thanks in advance. AttachmentWebNavigator.zip (36 Downloads) |
Last edited by: Ventouris at: 8/29/2016 2:37:10 PMLast edited by: Ventouris at: 8/29/2016 2:47:16 PM |
|
Follow us on