6/18/2009 8:28 AM | |
Joined: 5/28/2008 Last visit: 9/21/2024 Posts: 4515 Rating: (839) |
Hello, Please tell us the version of the installed ALM. And If it's V4.0, I think this thread will help you. Also this thread will help you too Regards, |
Ayman Elotaify |
|
6/18/2009 8:57 AM | |
Posts: 217 Rating: (52) |
Hello, I agree with AMAZINGAHMED it seems to be a problem with your graphics. One more thing is to conform it. Is that stick only content one key if yes most probably you will get two cross marks for two keys. Try to reinstall it. If it is not working you have to check your graphics in your PC. Best regards. |
6/18/2009 9:01 AM | |
Joined: 4/24/2006 Last visit: 9/20/2024 Posts: 8742 Rating: (1168) |
Dear nettogrisen, Perhaps you might try to install Service pack 2 for Automation License manager v4.0: http://support.automation.siemens.com/WW/view/en/114358 Perhaps these links might help: http://support.automation.siemens.com/WW/view/en/23174049 http://support.automation.siemens.com/WW/view/en/23174054 Best regards, Wizard |
6/18/2009 9:08 AM | |
Joined: 11/15/2006 Last visit: 5/7/2021 Posts: 1319 Rating: (172) |
Hi, AttachmentOLEfix_red_X.zip (413 Downloads) |
Have Fun! |
|
This contribution was helpful to1 thankful Users |
6/18/2009 10:42 AM | |
Posts: 3 Rating: (0) |
How on earth did you ever find this? Thank you very much, this is exactly what was needed. Kudos! Thanks to everyone who replied. |
9/25/2016 7:52 PM | |
Posts: 1 Rating: (0) |
dear support I've been following problems I Reinstalled the program again but the problem is not resolved see Picture1 alm_v5_3_sp2_upd2 is now install in my pc but I am faced with the following problem : see Picture2 please help me thanks AttachmentPictures.zip (300 Downloads) |
Last edited by: Min_Moderator at: 9/26/2016 2:47:24 PMRemove contact data and upload attachment |
|
Follow us on