9/25/2016 5:13 PM | |
Posts: 67 Rating: (7) |
i did came around some ideas. Ie. a motorstart counter, etc. (C3 and C4 would be removed, when in service) There's no need to reset a start counter. How would i prevent someone from pressing two buttons at the same time? Ie. Up and down at the same time? If two buttons are pressed, all outputs should go off. And another question, why can't i find a flag for green backlight? I've attached the LSC - I don't know why the cluttered text at B009/M28 shows up, thats new! EDIT: First i would buy a 6ED1052-1MD00-0BA8 It should be a 24V unit with display? After a second thought - I'd rather like an 6ED1052-2MD00-0BA8 + a TDE! controlpanel, 6ED1055-4MH00-0BA1 - Would they do the same? + I would get a nice display. AttachmentLift_control_V4_Expirimental.zip (197 Downloads) |
Last edited by: cs_dk at: 9/25/2016 6:57:46 PMLast edited by: cs_dk at: 9/25/2016 7:11:14 PM |
|
9/25/2016 8:21 PM | |
Joined: 12/18/2014 Last visit: 3/29/2024 Posts: 32631 Rating: (4044)
|
First: There is no flag for the green display. This is the normal background of the display without driving a backlight. If you take a logo with display or a logo without bisplay (but with a TDE) is irrelevant for the function. The key lock is incorporated in the attached program. And you have to finish all of the blocks with an output. In the simulation, this is not necessary, but you can not transfer the program to a logo. The transfer is canceled with an error message. AttachmentLift_control_V4_Expirimental_V2.zip (189 Downloads) |
9/25/2016 9:19 PM | |
Joined: 12/18/2014 Last visit: 3/29/2024 Posts: 32631 Rating: (4044)
|
6ED1058-0BA08-0YA1: 6ED1055-4MH00-0BA1: 6EP1332-1SH51: 6ED1052-2MD00-0BA8: AttachmentLift_control_V4_Expirimental_V3.zip (205 Downloads) |
9/26/2016 5:49 AM | |
Posts: 67 Rating: (7) |
Thanks, how ever. The pressure switch does not forbid I1 to execute anymore. And I3 (down) does not work. Will have a to look at it later this day. |
9/26/2016 6:07 AM | |
Joined: 12/18/2014 Last visit: 3/29/2024 Posts: 32631 Rating: (4044)
|
Sorry. I hope that now everything is working properly.
AttachmentLift_control_V4_Expirimental_V4.zip (211 Downloads) |
Last edited by: ixo65 at: 9/26/2016 6:07:36 AM |
|
9/29/2016 5:25 AM | |
Posts: 67 Rating: (7) |
It looks correct. The ordered items will arrive today, can't wait to get my fingers on it. Thanks a lot. |
This contribution was helpful to1 thankful Users |
Follow us on