9/27/2016 8:01 AM | |
Posts: 2 Rating: (0) |
Dear Sir, My PG 740P111 are damage. 1. Can i install Step 5 to window XP and run the system in virtual machine ? 2. I have the comunication cable6E5 734-1BD20 with D25 - D9.how can i use this comunication cable to connect to my laptop use USB. can i use USB-to-Serial Converter (D9 male to USB).
------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 9/28/2016 12:18:01 PMNew subject after splitting |
|
9/28/2016 2:47 PM | |
Joined: 3/30/2011 Last visit: 9/22/2024 Posts: 736 Rating: (256) |
yes, normally for s5 i use vmware machine with winxp. actually i have an usb-s5 interface but in the past i also use usb-serial converter with serial interface. Best Regards |
★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★ |
|
10/7/2016 8:10 AM | |
Posts: 92 Rating: (5) |
Step 5 software may not work on Virtual machine , but im sure you can't go online with your controller if you use anything except Com Port. regards |
Follow us on