4/24/2012 10:09 PM | |
Joined: 4/19/2008 Last visit: 2/9/2024 Posts: 1525 Rating: (159) |
Hello, I have Found One Document Related to Siemens HMI with other PLC, May be you have used the Same Cable which Mention in the FAQ, But you can Have a look on the RS 422 - RS 232 Converter.pdf also have a look on Why is no connection set up from the operator panel to the controller via interface IF1 A (IF1 B) (IF2)? As I have not Used Siemens HMI with other PLC yet, but Siemens PLC with Other HMI..... |
Ammy |
|
This contribution was helpful to1 thankful Users |
4/24/2012 11:27 PM | |
Joined: 5/28/2008 Last visit: 4/15/2024 Posts: 4505 Rating: (836) |
Hello, Have you seen this FAQ: Hope this helps.
|
Ayman Elotaify |
|
10/21/2016 2:16 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
New question published by Mahmoud.Hazem is split to a separate thread with the subject Get PLC Buss address from the CPU?. Best regards |
Follow us on