10/26/2016 8:53 AM | |
Posts: 3 Rating: (0) |
Hello This is a recent problem, after change the old crt display for a new digital, but i dont know how this can be affect, and did confirm this problem only occurs to the Z axis. In Diagnosis> PLC Status> EW , AW or MW i cant see the "QB84 and QB85" via control, maybe check connect with PC? And do not think anyone has touched the NC, for load backup. Attachment a video, this morning with the problem thank very much AttachmentIMG_1217.MOV (44 Downloads) |
10/27/2016 8:58 AM | |
Posts: 3 Rating: (0) |
i cant see the "QB84 and QB85" , how i can, do it? thank you |
Follow us on