1/13/2017 11:29 AM | |
Joined: 10/11/2006 Last visit: 9/18/2024 Posts: 5906 Rating: (804)
|
Hello Ronesh, An error comes with an F ahead, whereas a warning has an A. If it looks like°009, this means drive is ready to switch on. hence at p554 a signal from "0" ->"1" is required. The presetting of p554 is B22 which means that at the CUVCs -X101/9 must be 24V DC. After default setting and a wired setpoint, the drive must turn now. Some general information: The link to the compendium Masterdrives VC 3.4:http://support.automation.siemens.com/WW/view/en/13472409 The link to the commissioning tool DriveMonitor:http://support.automation.siemens.com/WW/view/en/11769381 The RS232 connection cable: 9AK1012-1AA00 PC - Masterdrives. See also section 5.5.1.2 Attachmentvc33_kurzba_e.pdf (237 Downloads) |
With best regards, |
|
Follow us on