1/15/2017 7:32 PM | |
Joined: 11/14/2016 Last visit: 10/4/2022 Posts: 3 Rating: (0) |
Hello I have a problem with Analog Input Module:6ES7331-7KF02-0AB0 I have 4 analog input and one analog output in my project the led sf is on but only with module that I connected with is Transmitter Isolator TG-AI-7021D5 the value of input is 777f and in output ther is no respone note: I do not connect all sensors in the field I attached the diagnostic error massages Could I have your advice Best of regards ------------------------------------------------------------------------------------------ AttachmentModule Information.pdf (197 Downloads) |
Last edited by: Min_Moderator at: 1/16/2017 2:24:34 PMNew subject after splitting |
|
Follow us on