1/22/2017 9:20 PM | |
Joined: 3/14/2008 Last visit: 9/23/2024 Posts: 2096 Rating: (937)
|
Hi, Virtualization is possible, but not for your setup I'm afraid. First, you will need at least PCS7 v7.1 SP2 and second you will need to use ESXi instead of VMWare. VMware is virtualization on the software level. You have a host OS and on the host a quest OS can be installed. This is not released by Siemens, but I also use VMware so I can engineer on a ES, but it is not wise to use this in a plant. Second is the ESxi and this is virtualization on the hardware level. There is no host OS in this case. This is released for PCS7, but as of v7.1 SP2. |
If I could help you, you can use the RATE button. Thank you. |
|
1/27/2017 8:07 AM | |
Joined: 8/19/2012 Last visit: 9/20/2024 Posts: 125 Rating: (0) |
Thank you for your reply. please help me for get a good solution.our system more slowly. |
Follow us on