4/11/2016 3:06 PM | |
Joined: 4/21/2015 Last visit: 4/19/2022 Posts: 18 Rating: (0) |
ya i have gone through the previous comments but got really confused for p1240 = 1 or 3 |
4/12/2016 6:10 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Hello, In principal, in hoist application, in case of hoist movment, either up or down, before release of motor hold brake, sufficient torque should be generated in motor which will hold the load at position so that it will not fall down. So I think, in your case these parameter setting is missing. Motor torque is not present to hold the load that is how, when inch up or down operation is selected, boom falls down. Please refer the attached sheet & try to set the parameters as recommended. This should solve your problem.
AttachmentHoist braking .pdf (350 Downloads) |
4/12/2016 8:23 AM | |
Joined: 4/21/2015 Last visit: 4/19/2022 Posts: 18 Rating: (0) |
thanks, i will check and come back |
4/17/2016 4:36 PM | |
Joined: 10/10/2010 Last visit: 4/28/2024 Posts: 307 Rating: (15) |
the Dc dynamic brake should be synchronized with the motion control system and the feed back encoder |
8/31/2016 8:30 PM | |
Posts: 4 Rating: (0) |
P1227 keep 4Sec P1120-5sec P1121-4Secs P1216-- 1200 P1217-- 3000 |
Follow us on