2/22/2017 8:35 AM | |
Joined: 8/1/2013 Last visit: 9/20/2024 Posts: 123 Rating: (9) |
Hi all: I want to ask to the masters about the stop D. I already have the machine (840d SL V4.7) with all the safety implemented. 36901 = 61H. My doubt is about how to execute correctly the Stop D. Right no my machine configuration simplify is un X carriage who move a system about 1000kg. The machine has Scanners to launch the stop D. The problem is when I cross the scanners and the stop D is active the machine even if the speed is about only 10m/min (60m/min is the maximun) the brake the control execute is very strong. is like the machine hit something. Then many alarms like contour monitoring apeard and finally the emergency is executed (Stop A). I dont really know which parameters define the time or the accel to execute this stop D. In normal process the scanners can be cross inn everytime and the machine should stop with a quickly deceleration but controled and with no risk. I put the backup for this axis. Somebody can tell me what is wrong or which parameters should I change? Thanks in advance¡¡¡ Attachmentax1 backup.txt (86 Downloads) |
2/22/2017 2:16 PM | |
Posts: 391 Rating: (50)
|
Is this your first safety commissioning? If so. You should contact the Siemens service. |
Follow us on