2/23/2017 9:00 PM | |
Posts: 1 Rating: (0) |
Hi Alex, I'm also on a MacBook Pro 15", and using parallels. Software works fine, but i am having trouble connection to the PLC via ethernet cable. There is no Ethernet port in the MacBook, so I am using a Thunderbolt adapter. In parallels i am using the bridged network (default adapter). I have managed to ping the PLC, when using fixed IP-adress (192.168.0.X), but i cant seem to connect through the TIA software. Any ideas to help me solve this issue? Thanks. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 2/24/2017 12:52:57 PMNew subject after splitting |
|
Follow us on