2/24/2017 5:34 AM | |
Posts: 7 Rating: (0) |
Hello everyone I explain my problem, I programmed my ob 10 to run an output every Thursday at 9:30. I took exactly the same example as the attachment. It works very well except that I have a problem on my reset because my output on the sfb4 block remains powered because my ob 10 remains powered. In my case I would like to be able to run my output every Thursday at 9:30 and for 20 seconds and then that it is stopped and that it resumes on the next Thursday at the same time. Attachmentexample.pdf (161 Downloads) |
2/24/2017 7:54 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1050) |
hi, I would use an Offdelay, like this: hope this helps, regards, |
FCK WAR! |
|
2/24/2017 9:51 AM | |
Posts: 7 Rating: (0) |
Thanks for the modification
but it does not work because I have the reset that starts when my ob10 is activated and the output of the cut is not 20 seconds.
I left my project as an attachment with the modification AttachmentInter__2.zip (95 Downloads) |
Last edited by: Min_Moderator at: 2/24/2017 1:28:47 PMAdjust formatting |
|
2/27/2017 3:23 PM | |
Posts: 7 Rating: (0) |
Thank you for your answer is what I expected and it works perfectly |
Follow us on